Hôm nay chúng tôi có thể giúp gì cho bạn?

Control Expert reports Integrity Check Warning at start up .

If ControlExpert_V140_HF1 is installed after ControlExpert_V140_HF_PMEPXM0100, then Control Expert will report following Integrity Check Warning at start up :

Warning can be ignored (click OK),  and Control Expert will start correctly.
A new Hot Fix : ControlExpert_V140_PMEPXM0100_HF0312169E will be distributed soon to fix this issue