Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
[Video] How to configure Remote Desktop Services on Rack PC Server and Magelis iPC Thin Client?
Goals and Symptoms
New Magelis HMIBMO and HMIBMI (running Windows 10) with Modular Display can be used as Industrial thin client in the plant field, especially for Rack PC server (running Windows Server) with SCADA Application.
The goal of this resolution is to provide the steps to follow in order to configure Remote Desktop Services on Rack PC Server and Magelis iPC Thin Client
Causes and Fixes
Here is the video to show How to configure Remote Desktop Services on Rack PC Server and Magelis iPC Thin Client