Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
PME 9.0 - New 3rd party device created with DTE does not work
Product Line
Power Monitoring Expert 9.0

Environment
DTE - Device Type Editor

Issue
The new devices created with DTE are not loading and you will see error messages in the System Log:

"Translator map file 'DEVICE_NAME.xml' not loaded due to previous error. Will retry."
"The attribute 'TimestampedByPlugin' on this element is not defined in the DTD/Schema." -
(or some other attribute as well)

Cause
The modbus-schema.xml file in the config/translator folder is an old version and does not contain the specific attribute referred by the error log.

Resolution
Replace the modbus-schema.xml file in config/translator with the one from system/translator folder or from a healthy PME system.