Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
After entering my username & password in the authentication window for Ecostruxure Power Build Rapsody , I get an error message/software crashes/software does not open. What should I do?

After entering my username & password in the authentication window for Ecostruxure Power Build Rapsody , I get the following error message & I cannot use the software

After entering my username & password in the authentication window for Ecostruxure Power Build Rapsody , I get an error message/software crashes/software does not open

1) Ecostruxure Power Build - Rapsody has undergone some improvements. One of the improvements is to authenticate users using a new registration & authentication mechanism.
To learn more about the new registration & authentication mechanism, you can refer to this FAQ -https://www.se.com/ww/en/faqs/FA378867/
2) If you get the above error message, there could be 2 reasons:
a) Your internet connection is not stable or slow.
b) You are using your laptop/desktop in an IT environment that has a Proxy Script Configured/Proxy configured.

Please check the attached Microsoft powerpoint which will help you to overcome this issue.

Schneider Electric Việt Nam

Phần đính kèm
EcoStruxure Power Build Rapsody - Resolution for authentication issue.pdf [496.42 KB]