Hôm nay chúng tôi có thể giúp gì cho bạn?

Is it possible to read Data Recorders via Modbus in ION9000 meter?

Product Line:
ION9000 meters

Description:
In ION9000 meter's Modbus register map, it is mentioned the registers for Data Recorders are from 53001 to 53153. The question is, what data is available in these registers?
The below screenshot is taken from High-Level Modbus Map sheet.
aa

Answer:
Data recorder access via Modbus is NOT supported for the ION 9000 meter. The Modbus map has reserved those registers for potential future use. It does not mean the meter supports reading data recorders.