What Modbus TCP Unit ID can be used to communicate to a BMXNOR0200 card?
Issue
When receiving Modbus TCPIP messages into the BMXNOR0200 and are any specific Unit IDs between 1-255 off limits?

Product line
Modicon X80

Resolution
Unlike the BMENOC03x1 modules which have Index 100 and 255 reserved, in the BMXNOR0200: 1-255 are available.



If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: