Issue
A Trend report is configured, generated, and then dowloaded as a pdf file. The pdf file includes a number of blank pages.
Product Line
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024
Environment
Web Applications - Reports
Cause
When a Trend report is configured to include a large number of measurements, if that report is downloaded in pdf format it will include a number of blank pages. This happens because of the way the reporting services handles wide tables. In the Trend report only graph is visible, but the blank pages get added to match the width of the table expansion even though the table is not visible.
Resolution
The known workaround is to limit the number of measurements to from one to six when configuring the report, to keep the tables smaller in width.
Đã phát hành cho: Schneider Electric Việt Nam