Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the speed limitation and bandwidth for ethernet backplane
  1. Issue
The speed limitation for X-BUS backplane is 12Mbps and customer would like to know the speed limitation & bandwidth  for Ethernet backplane.
  1. Environment
N/A
  1. Resolution
Ethernet backplane is 100Mbps full duplex. The bandwidth for each slot is as following:
  • Ingress rate limiting must be set to 0.1 Mbps for broadcast traffic.
  • Ingress rate limiting must be set to 1 Mbps for all other traffic.
  • Port egress rate limiting must not be set.
  1. FAQ Applicable Conditions
Any BMEXBP**** backplane