Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to delete recipes at runtime on the Magelis HMI?

Issue:
Looking for options on how to delete recipes created or downloaded to the Magelis HMI at runtime.

Product Line:
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer, there are a couple of ways in which we can delete a recipe during runtime on the Magelis HMI.

The first option is to make use of a "Delete" recipe button that you can drag onto the panel from the toolchest in Vijeo Designer. During runtime, when you select a recipe group and recipe, when you press the Delete button, it will delete the selected recipe from the list.

The second option is to write a script in an action or in a touch action script. The script will essentially write a value to the _RecipeDefaultControl.Operation variable. The value to trigger a delete is the value "16"

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)