Issue:
It is not clear how to setup a fill animation in EcoStruxure Operator Terminal Expert.
Product Line
EcoStruxure Operator Terminal Expert.
Resolution:
In EcoStruxure Operator Terminal Expert, it is possible to setup a Horizontal or Vertical fill animation. In order to find the correct property, you must follow the procedure below:
1) In your application, drag one of the objects found in the "Shapes" category from the "Toolchest" on to the screen.
2) Click on the object and goto the "Property Inspector"
3) Click on the "Shape" tab in the "Property Inspector"
4) Click on the "Size/Location" tab
5) Expand the "Animation" property
6) Find the "Hortizontal Size" or "Vertical Size" property
7) To the right of the corresponding property, click on the box.
8) Choose "Variable" to associate the "Size" property with a control variable.
9) Select the variable of your choice
10) Create a numeric display on the screen to manipulate the value of the control variable
11) Setting the value from 0-100 will gradually fill the object from 0% to 100%
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Đã phát hành cho: Schneider Electric Việt Nam