Configuration Manager Tool v9 fails while reading Power Monitoring Expert v9.0 system
Issue
Configuration Manager Tool v9 fails with below errors while Read from System’ in PME v9 machine.

||Warning||None||||Could not find manifest file: D:\1.PME 9.0 Configuration Management Tool\bin\MasterFileLists\PowerMonitoringExpert\9.0\DataCenter\en\config.csv||None
||Warning||None||||Could not find manifest file: D:\1.PME 9.0 Configuration Management Tool\bin\MasterFileLists\PowerMonitoringExpert\9.0\Healthcare\en\config.csv||None



Environment
Power Monitoring Expert v9.0 system read by Configuration Manager Tool v9.


Cause
When older PME versions are upgraded in-place this registry will remain and when cause this issue when old systems are DataCenter or Healthcare. From PME 9 onwards we don’t have any such PME versions anymore.

Resolution
Open RegEdit and go to the path > “HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\Power Monitoring Expert\9.0” and delete key "SolutionBuild" which contains value either 'DataCenter' or ' Healthcare'.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: