Hôm nay chúng tôi có thể giúp gì cho bạn?

Converted empty negated pins are shown with the label false after the Concept application is converted to Unity.

Issue
Converted empty negated pins are shown with the label false after the Concept application is converted to Unity.

Products Line
Unity

Environment
Windows 7, Windows 10

Resolution
When you convert a Concept application to Unity and the logic contains negated pins, some of the negated pins appear with the word 'False'.

The reason for the issue is due to the software design.  When Unity converts a section that contains logic with a pin that is negated and has no
connection link and no default value, the converter is designed to set the default value of the pin to "false".