Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Integrity check error is returned after running Control Expert following GPL Library install
Issue
Integrity check error is returned after running Control Expert following 'PSx GPL 2015 R2 for Unity Pro' Library install

Product Line
Control Expert

Environment
Windows 10.

Resolution
An integrity check error message gets returned after starting Control Expert 14.1 following the installation of the
'PSx GPL 2015 R2 for Unity Pro' library.

The issue can be resolved by performing the following steps:
  • Uninstall Control Expert 14.1
  • Reboot.
  • Delete the folder named ‘PSx GPL for Unity Pro’ from the folder named ‘C:\ProgramData\Schneider Electric\Control Expert 14.1'.  (Note: This folder does not get deleted by the uninstall, If a third party library is installed)
  • Install Control Expert 14.1
  • Install the hotfixes including HF1 (run Control Expert and close after each hot fix install.)
  • Install the ‘GPL_Communication’ family.
  • Run Control Expert 14.1
  • Close Control Expert14.1
  • Install the ‘GPL_Devices’ family.
  • Run Control Expert 14.1
  • Close Control Expert14.1
  • Install the ‘GPL_Diagnostics’ family.
  • Run Control Expert 14.1
  • Close Control Expert 14.1
  • Install the ‘GPL_Process’ family.
  • Run Control Expert 14.1
Note:

When you uninstall Control Expert, it should delete 'Control Expert 14.1 folder from both 'C:\ProgramData\Schneider Electric'  and
C:\Program Files (x86)\Schneider Electric.  If it doesn't, then you will need to manually delete them.