Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What does the [ION_Data]- MAINTENANCE-Job task do under Windows Task Scheduler?

Issue
What does the [ION_Data]- MAINTENANCE-Job task do under Windows Task Scheduler?

Product Line
Power Monitoring Expert (PME) 7.2.x
Power Monitoring Expert (PME) 8.x
Power Monitoring Expert (PME) 9.x
Power Monitoring Expert (PME) 2020
Power Monitoring Expert (PME) 2021
Power Monitoring Expert (PME) 2022
Power Monitoring Expert (PME) 2023
Power Monitoring Expert (PME) 2024


Environment
PME Software

Resolution
image of maintenance job

The ION_Data Maintenance job runs a powershell script which performs a defragmentation on ION_Data.  Details of the script can be found in
Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\cfg\DbScheduledTasks

Note: For large databases the function can take a long time to run which can slow down data insertion so at times it would be disabled to avoid this issue.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Phạm vi:
Tìm hiểu thêm
Sản phẩm: