Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Is it possible to transfer the ATV71 program to ATV930?

Article available in these languages: Czech, Tiếng Thái

Issue:
Wants to know if the old parameters of the ATV71 can be transferred to the ATV930?

Product Line:
Altivar ATV71 ATV930

Environment:
All

Cause:
Programming

Resolution:
No. The ATV930 has a different memory may and different capabilities than the older ATV71.
The program files are not compatible.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)