Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What are Manager, Module and Register names for External modules used in a translator file?
Issue
When modifying a translator in DTE, there is no External (Numeric, Boolean, Pulse) module in the Measurement Tree for linking to a newly created register in the Modbus Map.

Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
Device Type Editor

Cause
Using a control object in Vista requires an External (Numeric, Boolean, Pulse) module in the translator file. Sometimes it is necessary to modify the translator to add such a module.

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten.*

The ION extension file in the .../config/translators folder has the ION configuration for any custom translator.

1. The 'Manager' name doesn't matter, leave it as default.

2. Proper 'Module' names should be one of:
ExternalNumeric_Module
ExternalBoolean_Module
ExternalPulse_Module

3. Proper 'Register' names should be one of:
NumericVariable_Register
Boolean_Register
Pulse_Register
Enumerated_Register

An example for an External Numeric Module:

ManagerObj" t:H="160433152" t:P="2" t:N="Write to Numeric" t:CI="Manager_Module" t:MC="Universal_Module">

ModuleObj" t:H="160433153" t:P="160433152" t:N="Numeric" t:CI="ExternalNumeric_Module">

RegisterObj" t:H="160433154" t:P="160433153" t:N="Register 1" t:L="Reset Energy" t:CI="NumericVariable_Register"/>