Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the recommended type of Ethernet cables to be used by M580 and Quantum ERIO?

Issue
What is the recommended type of Ethernet cables to be used by M580 and Quantum ERIO?

Product Line
Modicon M580, Quantum, x80 Modules

Environment
BMEP586040, BMECRA31210

Resolution
Schneider Electric has guidelines when making cables connections between remote I/O devices on a Quantum and M580 EIO installation. It is recommended to use shielded twisted pair CAT5e  (10/100 Mbps) cables that complies with TIA/EIA-568 standard and IEC11801 /  EN 50173 class D to protect against the most severe disturbance.

You can find this information on the documents below: