Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
NetBotz 250 | Adjusting Temperature/Humidity Sensor Thresholds
Issue:
Process for adjusting sensor thresholds on the NetBotz 250.

Product Line:
NetBotz 250 (NB250)

Environment:
NetBotz 250 (all versions)
Universal Sensors (Temperature, Humdity, etc)

Resolution:

Adjusting Wired Temperature/Humidity Sensor Thresholds
1) Log into the NetBotz 250 web interface.
2) Configuration Menu > Device > Wired Sensor > Temperature & Humidity
3) Click on the Name of the sensor.
4) Click on the Threshold Settings link to adjust: Maximum, High, Low, Minimum, or Hystersis.
Click on the Rate of Change Settings link to adjust the short term and long term increasing/decreasing thresholds.
5) Adjust the Thresholds and click Apply.

A similar process can be followed for all other sensor types: Dry Contact Inputs, Smoke, Vibration, Fluid Detector, & Door Sensors.  Wireless Sensor thresholds can be adjusted using a similar process under Configuration > Device > Wireless Sensor Network.