Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Can I preprogram IP address of the Profinet Communication Module (VW3A3627) for the ATV320 and install into another ATV320?
Issue:
Is the IP address retained in the VW3A3627 for the ATV320 drive?

Product Line:
Altivar ATV320

Environment:
All serial numbers, all model numbers

Cause:
Customer want to have a preprogram IP address on Profinet Communication module (VW3A3627) so he didn't have to program when installed into the drive.

Resolution:
No, you cannot preprogram the IP address for the Profinet Communication Module (VW3A3627) because the address is not retained in the Card.