Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to resolve the issue that occurs when the user tries to transfer a Control Expert application into an M580 PLC that contains a lower exec firmware version.
Issue
This video demonstrates the issue that occurs when the user tries to transfer a Control Expert application into an M580 PLC that contains
a lower exec firmware version.

Product Line
Control Expert

Environment
Windows 10

Resolution
This video demonstrates the issue that occurs when the user tries to transfer a Control Expert application into an M580 PLC that contains
a lower exec firmware version.