Issue
How to solve the Green screen/virtual screen issue ?
Sometimes, after a box wake up, a green screen can be displayed.
This is a virtual screen created by the Intel HD graphic as a extended desktop (the wallpaper can be different)
Product Line
Magelis HMIBMP IPC box
Environment
Win10 RC6.4
Resolution
Update the card graphic driver in v15.40 (or more):
Intel Graphic Driver v15.4
Đã phát hành cho: Schneider Electric Việt Nam