Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Can you download a different version of SoMove Configuration file in Altivar Process VFD?
Issue:
Can SoMove Software download an older Configuration file in to the VFD?

Product Line:
ATV630 , ATV930

Environment:
Altivar

Resolution:
You can download a SoMove Conf with version N to a drive with version N or N+1 or greater. but you can't transfer it to a drive with version N-1 or less.

You have 2 solutions inthe example below:

1.    You can modify the version of the offline conf, by changing the Topology.
Drive screen shot

Then click ok when SoMove displays message.

warning screenshot
After that, transfer the conf with version V2.2 to a drive with version V2.2.

Or

2.    Update the drive to the version V3.1 before transfer. Then you can perform conf transfer.