Hôm nay chúng tôi có thể giúp gì cho bạn?

Is it possible to use Resi9 MP on hollow wall?

Issue :
Installation of an enclosure Resi9 MP in a hollow wall.

Product Line :
Resi9 MP

Cause :
IEC 60670-1 standard constraint

Resolution :
Yes it's possible to use Resi MP on hollow wall, because we have a dedicated version with back part in GWT850 as requested by standard for hollow wall installation.

Note :
To select the right enclosure, please chose the commercial reference starting with MIP21, it contains hollow kit installation.
if you need a spare part for the hollow wall kit please refer to MIP99047.
Instruction Sheet of the hollow wall kit : BBV48374
Video : Resi9 MP - Flush Version Installation