Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to select replacement for XPSAR

Article available in these languages: Tiếng Hà Lan

XPSAR is replaced by XPSUAF + XPSUEP - 24V
XPSAR replacemrent
Commercial ReferenceReplacement Commercial Reference
XPSAR311144XPSUAT13A3AP
XPSAR311144PXPSUAT13A3AP

Replacement/substitution according to the terminal connector:
Terminal connections
XPSAR is replaced by XPSUAF + XPSUEP - 115VAC and 230VAC
XPSAR replacement 115 and 230VAC
Commercial ReferenceReplacement Commercial Reference
XPSAR351144XPSUAF33AP + XPSUEP34AP
XPSAR351144PXPSUAF33AP + XPSUEP34AP
XPSAR371144XPSUAF33AP + XPSUEP34AP
XPSAR371144PXPSUAF33AP + XPSUEP34AP

Replacement/substitution according to the terminal connector:
Terminal connections
Wiring Emergency Stop diagram XPSAR & XPSUAF + XPSUEP

E-Stop wiring

Wiring Emergency Stop single channel diagram XPSAR & XPSUAF + XPSUEP
E-Stop wiring
E-Stop wiring

E-Stop wiring
E-Stop wiring
E-Stop wiring

Wiring Emergency Stop in series diagram XPSAR & XPSUAF + XPSUEP
E-Stop wiring
Definitions of pins

Wiring Safety Switch diagram XPSAR & XPSUAF + XPSUEP
Safety switch wiring
Safety switch wiring
Safety switch wiring

XPSAR range can be replaced either by the combination of XPSUAF + XPSUEP ranges or by the XPSUAT range, according to the below number of contracts:

XPSAR range
It has 7 safety NO outputs + 2 single NC outputs

XPSUAF + XPSUEP ranges
The combination has 7 safety NO outputs + single NC outputs

XPSUAT range
It has 6 safety NO outputs + 1 safety NC output

XPSAR is replaced by XPSUAT - 24V
XPSUAT replacement
Commercial ReferenceReplacement Commercial Reference
XPSAR311144XPSUAT13A3AP
XPSAR311144PXPSUAT13A3AP

Replacement / substitution according to the terminal connector:
Terminal connections

XPSAR is replaced by XPSUAT - 115VAC and 230VAC

Wiring diagram
Commercial ReferenceReplacement Commercial Reference
XPSAR351144XPSUAT33A3AP
XPSAR351144PXPSUAT33A3AP
XPSAR371144XPSUAT33A3AP
XPSAR371144PXPSUAT33A3AP

Replacement / substitution according to the terminal connector:
Terminal connections

Wiring Emergency Stop diagram XPSAR & XPSUAT
E-Stop wiring

CAUTION

The information provided in this documentation contains general descriptions and/or technical characteristics of the performance of the products contained herein. This documentation is not intended as a substitute for and is not to be used for determining suitability or reliability of these products for specific user applications. It is the duty of any such user or integrator to perform the appropriate and complete risk analysis, evaluation and testing of the products with respect to the relevant specific application or use thereof. Neither Schneider Electric nor any of its affiliates or subsidiaries shall be responsible or liable for misuse of the information contained herein. If you have any suggestions for improvements or amendments or have found errors in this publication, please notify us.

You agree not to reproduce, other than for your own personal, noncommercial use, all or part of this document on any medium whatsoever without permission of Schneider Electric, given in writing. You also agree not to establish any hypertext links to this document or its content. Schneider Electric does not grant any right or license for the personal and noncommercial use of the document or its content, except for a non-exclusive license to consult it on an "as is" basis, at your own risk. All other rights are reserved.

All pertinent state, regional, and local safety regulations must be observed when installing and using this product. For reasons of safety and to help ensure compliance with documented system data, only the manufacturer should perform repairs to components.

When devices are used for applications with technical safety requirements, the relevant instructions must be followed.

Failure to use Schneider Electric software or approved software with our hardware products may result in injury, harm, or improper operating results.

Failure to observe this information can result in injury or equipment damage.

© 2021 Schneider Electric. All rights reserved.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: