What is the purpose of the PrismaSeT Active wiring kit?
- It powers the wireless panel server.
- It provides the connection points for the voltage presence indicators.
- It protects the wires with fuses as close as possible to the connection to protect equipment and people in case of insulation damage or broken wires (direct contact on active parts).
- Traditional wires don’t provide protection between their connection and the measuring device. The wiring kit integrates fuses that ensure this function.
- The wiring kit provides a standard solution (universal supply for the PrismaSeT offer) designed for this purpose.
- The wiring kit preserves useful space in the panel for the customer because it does not require an extra fuse holder or circuit breaker.
- Thanks to the provided connector and the marking on the wires, you cannot confuse the different phases.
If you are looking for further information regarding the steps to follow when installing the wiring kit, watch this video:
https://www.youtube.com/watch?v=Du8xGHIu9M4
You can also access this instruction sheet:
https://download.schneider-electric.com/files?p_enDocType=Instruction+sheet&p_File_Name=NNZ50846-01.pdf&p_Doc_Ref=NNZ50846