Hôm nay chúng tôi có thể giúp gì cho bạn?

Why is Unity Dif V14 SP2 not able to compare SFC program written in a POU section in Control Expert ?



Issue:

Unity Dif V14 SP2 unsupported comparison


Product Line:

Unity Dif V14 SP12, Control Expert, Unity Pro


Resolution:
SFC program comparison is not supported under POU section of a Control Expert project.