Hôm nay chúng tôi có thể giúp gì cho bạn?

How to import a BMXNOR0200 configuration into a BMENOR2200

How to import a BMXNOR0200 RTU configuration into a BMXNOR2200.

This video will demonstrate how to import a BMXNOR0200 RTU configuration
into a BMENOR2200 configuration. This can be applied to migrating an M340
application to an M580 application. The steps in this video will show:
1.) Creation of the M580 project
2.) Adding a BMENOR2200 to the M580 rack.
3.) Configuring the BMENOR2200 using the DTM Browser


Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: