Hôm nay chúng tôi có thể giúp gì cho bạn?

Where can I find information on the ATV630 power terminal conductor sizes?

Issue:
ATV630 Power terminal conductor size charts.

Product Line:
ATV630

Environment:
All

Cause:
Information needed for sizing conductors.

Resolution:
The power terminal data for the ATV630 drive can be found in the ATV630 installation manual under "Characteristics of the Power Part Terminals" section.

Link to the ATV630 installation manual: https://www.se.com/us/en/download/document/EAV64301/