What are the minimum and maximum ohm values for braking resistors for the ATV930 drives?
Needs ohmic values for ATV930 braking resistors.
Product Line:
ATV930
Environment:
230V up to 75KW, 480V up to 310KW, 600V up to 75KW, 690V up to 90KW.
Cause:
None.
Resolution:
See the attached document showing Min. and Max. ohm values.