Hôm nay chúng tôi có thể giúp gì cho bạn?

How to reduce motor noise when driven by an ATV320?

Issue:
The motor is quite noisy while running

Product Line:
ATV320

Environment:
ATV320 all series

Cause:
ATV320 is creating too much motor noise.

Resolution:
Options include:

Set noise reduction (nrd) to yes.  This creates a random frequency modulation which helps prevent a resonance.
Conf > FuLL > drC- > nrd = YES

Increase the switching frequency (SFr).  This may also increase the heat generated by the drive.
Conf > FuLL > drC- > SFr: (there is a range between 2 to 16kHz depending on the drive size).

Consider mounting characteristics to a machine.  Use mechanical joints (silent block) between the motor and the frame of the machine. It will help to suppress low frequency vibrations.