Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Can I use the READ_REMOTE EFB to read data from located or unlocated variables in a Unity Quantum PLC?
Issue:
Using the READ_REMOTE EFB to read data from located or unlocated variables in a Unity Quantum PLC


Product Line:
EcoStruxure Control Expert, Modicon Quantum


Resolution:
Yes. The READ_REMOTE block will read data from a remote Unity Quantum PLC that support the Data Dictionary feature  In the Quantum PLC, Data dictionary must be enabled. You must also de-activating the type verification based on checksum comparison using the CTRL parameter. In the second word of the four word array variable for the CTRL, you must enter a value of 1 to de-activate.

Quantum PLC showing unlocated variables with data.

read_remote_Quantum2.PNG


M580 with READ_REMOTE block receiving the unlocated data from the Quantum
read_remote_Quantum1.PNG