Issue:
Can you turn off the ILF internal communications fault on the ATV320 drive?
Product Line:
ATV320 Drive with an option card installed.
Environment:
All
Cause:
Connection issue between the option card and the Drive.
Resolution:
No you can not turn off this ILF fault detection. You will get the fault if the option card and the drive stop communicating.
Also note that the drive has to be power cycled to clear the fault.
Đã phát hành cho:Schneider Electric Việt Nam