Issue:
ATV212 Receiving 0-10v speed reference and does not run
Product Line:
ATV212
Environment:
0-10v speed reference
Cause:
n/a
Resolution:
First would check the start/stop signal. If 2-wire control, Cnod -should be 0. Make sure there is 24v at the F terminal. Then check Fnod for the speed reference ( VIA or VIB).
Make sure SW100 switches are set properly (for Voltage). Then can check the scaling parameters ( VIA: F201-F204, VIB: F210-F213). Would also check the run permissive circuit (F110 and F112).
Đã phát hành cho:Schneider Electric Việt Nam