Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
The Customer Experience Improvement Program (CEIP) in PowerChute Business Edition creates a sessions folder in the installation directory
Issue:
The Customer Experience Improvement Program (CEIP) in PowerChute Business Edition creates a sessions folder in the installation directory.

Product Line:
PowerChute Business Edition versions 10.0.4 and above

Environment:
All supported Windows and Linux operating systems

Background:
PowerChute creates a sessions folder in the installation directory when CEIP is enabled. When attempting to contact the Analytics Server, PowerChute generates 4 files in this folder. If communications between PowerChute and the Analytics Server are not established, PowerChute will attempt to contact the server every 7 days. Each time PowerChute attempts to contact the server, the 4 generated files are overridden.

Solution:
These generated files will automatically be deleted when PowerChute gains communications with the Analytics Server.