Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How are managed the reconnection timeouts in EcoStruxure Secure Connect Advisor?
In EcoStruxure Secure Connect Advisor, there are two levels of timeouts. This article will provide explanation about reconnection timeouts when a remote connection is established from a LinkManager to a SiteManager agent

This article is application for EcoStruxure Secure Connect Advisor, all versions

There are 2 levels of timeout in the Secure Connect solution :

- In the GateManager web UI, when logged in as a Basic Administrator, once a customer domain is selected in the left view, in the tab "Domain", section "Domain Settings", the Parameter "Keep-Alive Interval" is responsible for the duration after which a SiteManager (or LinkManager) is considered disconnected from the GateManager : after 3 times "Keep-Alive Interval" has elapsed, the SiteManager (or LinkManager) will be considered disconnected, thus resulting in a red flag icon being displayed next to the SiteManager (or LinkManager) being disconnected.
Once disconnected, the SiteManager (or LinkManager) will keep on retrying to connect to the GateManager.
There is no maximum number of attempts.
Annotation 2021-11-25 112544.jpg


- Once a remote connection is requested by a LinkManager user to a remote SiteManager agent, by clicking on the button "Connect" in the GateManager web UI, if connectivity between LinkManager and GateManager gets lost, the LinkManager will start a 15-minute (hardcoded value) timeout.
If the connectivity between LinkManager and GateManager is not recovered within this time interval, then the remote connection will be considered as lost by the LinkManager. Thus, a reconnection of the LinkManager to the GateManager after the 15-minute timeout will require the LinkManager user to manually re establish the remote connection, by clicking on the button "Connect" in the GateManager web UI.

Annotation 2021-11-25 112545.jpg