Hôm nay chúng tôi có thể giúp gì cho bạn?

Increasing the efficiency of Alarm Server operations by enabling Extended Memory Mode

This document explains User on how to increase the efficiency of Alarm Server in case of Large scale Projects/Projects with heavily loaded alarm tags.

By default Extended Memory Mode is set to FALSE and the Alarm Server runs on 32bit. This setting works for most of the small & Medium scale projects.

In case of Large scale Projects, this may not be enough and user can see intermittent Crashing of Alarm Server due to reaching its 4GB limit and also user can observe Alarm Query handling is also getting slow.

In order to tackle this, User has to enable the "Extended Memory" Mode to True as shown in below screenshot. This setting will be available in Supervision Project -> Services->Alarm Server.

Alarm

This setting allows the Alarm server process to utilize memory beyond a 4GB limit. It does this by running the process in 64-bit.

Extended Memory Mode enables efficient query handling for the alarm server process under the following circumstances:
a. On systems with a large archive of historic alarm data.
b. On high-capacity systems that can generate a large number of alarms.

This document is applicable for all versions of Ecostruxure Process Expert software. However the setting is exposed to Ecostruxure Process Expert from HDCS2019 onwards and for the previous versions, user has to do it in refinement mode of supervision project.