How to set Timeout Value for Modbus TCP/IP driver in Vijeo Designer 6.2?
You can use the driver property @prop:0 to set timeout value for Modbus TCP/IP driver in Vijeo Designer 6.2. Use this parameter to set a timeout value between 2 to 15 seconds for this driver. The timeout value determines the amount of time the driver takes to attempt a reconnect after a detected connection loss. Write an integer value from 2 to 15 to @prop:0 to set the timeout value.
Đã phát hành cho: Schneider Electric Việt Nam