Tìm các câu hỏi thường gặp
What is the maximum number of Modbus TCP client connection supported by the MC80 PLC?
Issue:
Number of Modbus TCP client connections supported by the MC80 PLC
Product Line:
MC80, EcoStruxure Control Expert
Resolution:
The MC80 PLC support 4 Modbus TCP client connections
Number of Modbus TCP client connections supported by the MC80 PLC
Product Line:
MC80, EcoStruxure Control Expert
Resolution:
The MC80 PLC support 4 Modbus TCP client connections
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: