Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to run safety task automatically after power cycle in M580 safety CPU ?
Issue
How to run safety task automatically after power cycle in M580 safety CPU ?

Product line Envirovment
Control Expert, Unity Pro, Modicon M580 safety

Environment
Windows 10 64 bits ,Windows Server 2019 64 bits

Resolution
A warm start causes each process task – including the (MAST, FAST, AUX0, AUX1) tasks – to re-enter its operating state as of the time of the power interruption. By contrast, a warm start causes the SAFE task to enter the STOP state, unless Automatic start in RUN is selected.

snap1.JPG