PME2021/PME2020CU2 ION Virtual Processor Modbus Slave. Transmit delay does not accept values within the valid range
Section 1 – Product /System/Environment information

PME2020 CU2
PME2021

_____________________________________________________________________________________
Section 2 – Issue
In PME 2020 CU2/PME2021 system, on virtual processor setup when changing transmit delay we get errors about delay to need to be between 10-6000 and we are using numbers in that range.
Tried 40, 20, 60, and nothing tried 100 and it took tried to switch back to 50 and would not take.
image.png
_____________________________________________________________________________________
Section 3 – Steps to Reproduce the Issue /Investigation/
  • On a PME2020, Open MC -> System-ION Virtual Processor Setup
  • Under a VIP. Example VIP. Default Add a port below Modbus Network/SlavePorts
  • Select MODTCP
  • Modify the settings set the "Transmit Delay (ms)" from 50 to 20, 40 or 60



_____________________________________________________________________________________
Section 4 – Root Cause
Confirmed issue

_____________________________________________________________________________________
Section 5 – Troubleshooting/Proposed Solution
The workaround is to edit manually the  file "vipsys.dat" to set up the desired  Transmit delay within the valid range
Will be located at
"C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\cfg\vip\VIP.NAME"


Example below:
Once you save the file if you open the ION Virtual Processor setting in MC will show the changes.
The VIP.NAME needs to be restarted.

Schneider Electric Việt Nam