Issue:
Diagnostic LED for the BMEAHI0812 and BMEAHO0412 Hart modules
Product Line:
BMEAHI0812, BMEAHO0412
Resolution:
Use the combined states of the RUN, ERR, I/O, BS, An and Hn LEDs to diagnose the channel and module status for the BMEAHI0812 and BMEAHO0412 modules:

Diagnostic LED for the BMEAHI0812 and BMEAHO0412 Hart modules
Product Line:
BMEAHI0812, BMEAHO0412
Resolution:
Use the combined states of the RUN, ERR, I/O, BS, An and Hn LEDs to diagnose the channel and module status for the BMEAHI0812 and BMEAHO0412 modules:
Đã phát hành cho: Schneider Electric Việt Nam