Can type K cable be used on our ATV212 drive
Issue:
Wants to use type K cable on the ATV212 drive.
Product Line:
ATV212
Environment:
All
Cause:
N/A
Resolution:
Unfortunately, we did not test this kind of cable with our product.
The main issue with the K cable type is the cross section of the cable strand is AWG30. This section is lower than the IEC version we tested in verification and validation test.
Risk is to break some strand when we tighten to the torque specified.
Test in our labs are done with the following cable:
- Class 5 IEC60228
- Class C UL486A
So, we can not guarantee the safety with type K cable.
Đã phát hành cho: Schneider Electric Việt Nam