Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why does my WebVisualization for a Text Display not display values when I try to display Binary for a Byte variable using the %b notation??
Issue
Why does my WebVisualization for a Text Display not display values when I try to display Binary for a Byte variable using the %b notation?

Example:
When a Text Field is configured to display Binary of my BYTE variable "SR_Main.a"
in EcoStruxure Machine Expert with the Text = %b like the image below,
Text field %b - Binary value display for BYTE variable

When the project is run, the result is that a static "%b" is shown and not the binary representation of the Variable:
Text field shows static "%b" instead of a dynamic binary value


Product Line
EcoStruxure Machine Expert

Environment
Codesys Web Visualization engine for Modicon M241/M251/M262 PLCs

Cause
The use of %b requires a Visualization Task and the addition of a WebVisualization node under the Visualization Manager.

Resolution
Here are the steps to add a Visualization:

1) In the Applications Tree tab, Right-click on the Task Configuration node, hover your mouse over "Add Object >" and click on "Task..."
Add Object > Task...
2) In the Add Task dialog, rename the Task to "VISU_TASK"
Rename the task to VISU_TASK
3) Click the Add button. As a result, you should see the new VISU_TASK created under the Task Configuration node:
VISU_Task appears in the Application Tree under Task Configuration node

4) Navigate to the Tools Tree, and right-click on "Visualization Manager"
5) Hover your mouse over "Add Object >" and click on "WebVisu...". Use the default name "WebVisualization" and click Add.
Add WebVisualization object under Visualization Manager
As a result, you should see two new nodes appear.
a) Under the Task Configuration -> VISU_TASK, you should see a new "VisuElems.Visu_Prg" POU call automatically created.
b) Under the Visualization Manager node, you should see the new "WebVisualization" node.
Newly created VisuElems.Visu_Prg and WebVisualization nodes appear
6) Download and Run your project

The result will be that the Text object will now show the Binary representation of the BYTE variable:
Result - Dynamic binary value now appears instead of the static %b


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)