Issue:
Requesting the trip curve for the motor overload protection feature of the Altivar drives.
Product Line:
ATV12 ATV212 ATV320 ATV340 ATV600 ATV900
Environment:
All models
Cause:
Estimating trip time
Resolution:
All of the Altivar drives provide motor overload protection based on standard IEC947-4 and therefore use the same trip curves. Please see the attached file.
Đã phát hành cho: Schneider Electric Việt Nam