Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
AP9520TH Not Showing in the Netbotz 750/755 Web Interface

Issue: AP9520TH Not Showing in the Netbotz 750/755 Interface

Product:
Netbotz 750
Netbotz 755

Environment:
Netbotz 750/755 - Any firmware
AP9520TH – Any Serial Number

Cause:
Connecting an AP9520TH with default DIP switch settings (all switches down. A-link address = 1, refer to below screenshot) will not show on the Netbotz Home page.
Alink Address
The AP9520TH is powered and displays temperature and humidity values.
A repeated error in the log will show.
2022-05-26 09:16:45.030+0800 [Thread-37] ERROR com.se.nb.nativeio.messages.DeviceId:-1 - Enclosure type AP9520TH cannot be on enclosure number 0
2022-05-26 09:16:47.000+0800 [Thread-43] ERROR com.se.nb.nativeio.messages.DeviceId:-1 - Enclosure type AP9520TH cannot be on enclosure number 0
2022-05-26 09:16:50.179+0800 [Thread-43] ERROR com.se.nb.nativeio.messages.DeviceId:-1 - Enclosure type AP9520TH cannot be on enclosure number 0

Resolution:
Start the DIP switch address to #2, refer to the screenshot above or the AP9520TH manual.  The AP9520TH sensor should now be available in the Netbotz 750/755 Home page.  A restart may be required.
The link address set on the AP9520TH will be minus 1 on the Identifier in the Netbotz web interface.

Example:
The DIP switch setting for this AP9520TH (see first image) is set on Address 2, but the Identifier is shown as 1 on the web interface.  The second AP9520TH DIP switch setting is for Address 3, and the identifier is shown as 2.
Example 1Example 2

If your Netbotz 750 is using 8 x AP9520TH, use the DIP switch settings below.
Dip Switch Setting

Please note this issue will be resolved in Botzware version 5.3.5

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: