Hôm nay chúng tôi có thể giúp gì cho bạn?

How do I update the firmware of my SRC series Smart-UPS?

Article available in these languages:

  • Tiếng Tây Ban Nha

Issue: There are two methods to update the firmware of Smart-UPS SRC models:

  • locally, via Serial connection only using the Firmware Upgrade Wizard v4.3.1.1_SRC application
  • remotely via the Network Management Card (NMC)

Note: The download link for the Chinese translation of this FAQ article is available at the end of this document..

If a previous version of the Firmware Upgrade Wizard or Firmware Images are installed, delete the old version and download the version attached to this article.

The download links for the necessary files can be found at the end of this document.

Product Line: SRC5KUXI, SRCE6KUXI, SRC6KUXICH, SRC10KUXI, SRC10KUXICH

Environment:

The system requirements for the Firmware Upgrade Wizard v4.3.1.1_SRC are as follows:
Operating systems: 64-bit Microsoft Windows 7, Windows 2016, Windows 8.1, Windows 10

To find the current UPS Firmware version via the UPS LCD display:
The Firmware Upgrade Wizard will detect the current version.
Alternately, from the main menu of the UPS LCD screen, select "About" and scroll down to "UPS Firmware".

To find the current UPS Firmware version via Firmware Upgrade Wizard:
Run the Firmware Upgrade Wizard and it will identify the current firmware version before performing the update.

To find the current UPS ID:
Every Smart-UPS has a unique UPS ID. This can be found in the "About" menu on the UPS LCD screen, or in the NMC web interface.

  • Follow the link the video guide on How to locate the UPS ID for APC Smart-UPS
  • The same models of UPS may have different UPS IDs depending on when they were produced.
  • The final firmware version will be determined by the UPS ID and not the Model Number of the UPS.
  • If the UPS ID is not listed in the below table, it does not have an update available.
  • The Firmware Upgrade Wizard will select the correct version for the unit you are updating.

Note: it is not recommended to perform a firmware downgrade to a lower firmware version than the current UPS firmware.

UPS IDUPS ModelLatest Firmware FileFirmware Version After Update
1006SRC5KUXISRC5KUXI_ID_1006_UPS_14-0.encUPS 14.0
1006SRCE6KUXISRCE6KUXI_ID_1006_UPS_14-1.encUPS 14.1
1006SRC6KUXICHSRC6KUXICH_ID_1006_UPS_14-2.encUPS 14.2
1011SRC10KUXISRC10KUXI_ID_1011_UPS_14-0.encUPS 14.0
1011SRC10KUXICHSRC10KUXICH_ID_1011_UPS_14-1.encUPS 14.1



Resolution:

UPS Firmware Update Instructions

IMPORTANT:

  • The UPS output must be turned off before the UPS firmware update
  • The UPS must be connected to AC input
  • The UPS battery must remain connected during the UPS firmware update
  • The serial cable, part number 940-8311 or 940-1525, supplied with the UPS must be used

Verify the hash key of the Firmware Upgrade Wizard after downloading. The current hash value is c0dee62920c76e617f746a628bc1b0a6.

  1. Open Command Prompt.
  2. Change the directory to the folder where the downloaded Smart-UPS_Firmware_Upgrade_Wizard_v4.3.1.1_SRC.exe was saved:
    • This is typically done using the "cd" command
    • For example, if the Smart-UPS_Firmware_Upgrade_Wizard_v4.3.1.1_SRC.exe file was saved to the Downloads folder, the command may look like: "cd C:\Users\Username\Downloads", or "cd Downloads"
  3. Run the command "certutil -hashfile Smart-UPS_Firmware_Upgrade_Wizard_v4.3.1.1_SRC.exe MD5"
  4. Compare and verify that the displayed hash value corresponds to c0dee62920c76e617f746a628bc1b0a6.

Example:

hash

UPS Firmware Update using the Firmware Upgrade Wizard:

Step 1A
:

  • Turn off the UPS output, and connect the DB-9 to RJ45 cable part number: 940-8311 or 940-1525,  between the UPS and the computer used to update the UPS firmware.
  • Download and unzip Smart-UPS_Firmware_Upgrade_Wizard_v4.3.1.1_SRC.exe
  • Identify and download the applicable UPS firmware file for the UPS model you are updating from the above table. Save the files on a local drive.

Step 2A:

  • Double click the extracted FirmwareUpgradeWizard.exe
  • Ensure that the Firmware Upgrade Wizard version shown is 4.3.1.1.80643 and select "Next":

FUW2A

Step 3A:

  • Select "Next" after checking the "I agree to terms in the License Agreement" checkbox:

FUW3A

Step 4A:

  • Choose the computer's communication port the UPS communication cable is connected to, and select "Next":

FUW4A

Step 5A:

  • The Wizard will check for UPS compatibility.
  • Select "Next" once compatibility has been confirmed:

FUW5A1
FUW5A2

Step 6A

  • Select "Browse", then select the UPS firmware file:
  • Note: refer to the above table to identify the correct UPS firmware file

FUW6A

Step 7A:

  • Select "Next":

FUW7A

Step 8A:

  • The UPS firmware is getting updated:

FUW8A

Step 9A:

  • Select "Finish" once the firmware update is completed.

FUA9A

Step 10A

  • Verify the UPS firmware version in the About menu on the UPS LCD Display

IMPORTANT: after the UPS firmware update is completed, the UPS LCD may display “Communication Error”. Follow the below steps to clear the alarm:

  • Turn off and unplug UPS from AC mains supply.
  • Disconnect the battery.
  • Reconnect the battery, reconnect the UPS to AC mains supply, and turn on the UPS. The UPS will now work normally with the updated firmware.
  • You can now turn the UPS output back on.



UPS Firmware Update using the web interfance of the Network Management Card (NMC):

NOTE: When performing the UPS firmware update using the NMC web interface, while connected to the web interface over Wi-Fi, a different network, or VPN, a file transfer timeout may occur if an HTTPS connection is used. Refer to FAQ000234317 for alternative methods to update the UPS firmware using the NMC.

Step 1B

  • The UPS output must be turned off before initiating the UPS firmware update. Ensure that network access is not dependent on the UPS for power, when updating via the Network Management Card.
  • If network access is dependent on the UPS for power, refer to Step 1A to Step 10A for instructions on updating the UPS firmware using the Firmware Upgrade Wizard.
  • If network access is not dependent on the UPS for power, ensure the attached load is correctly shut down before proceeding with turning off the UPS output.
  • To turn off the UPS output, from the NMC web interface choose “Control”, then “UPS”:

how to turn off UPS output

confirm turn off UPS output

Step 2B

  • Check if you have a Network Management Card 2 running Smart-UPS / Matrix Application, or a Network Management Card 3 running Smart-UPS Application, and ensure there are no active alarms reported.
  • Network Management Card 2 running Smart-UPS / Matrix Application:

NMC2

  • Network Management Card 3 running Smart-UPS Application:

NMC3

Step 3B

  • If using Network Management Card 3, go to Step 4B.
  • If using Network Management Card 2: Verify the firmware revision of your Network Management Card. From the NMC web interface choose “About”, then “Network”. The firmware must be v.6.4.0 or higher, but we recommend you always run the latest available NMC firmware. To update the firmware of your Network Management Card, refer to FA156047 .

how to check NMC FW

Step 4B

  • Download and run Smart-UPS_Firmware_Upgrade_Wizard_v4.3.1.1_SRC.exe to extract the Firmware Files
  • After the extraction is complete, you can close the Firmware Upgrade Wizard by pressing Cancel
  • To view the extracted firmware files, go to C:\Users\Username\Documents\Smart-UPS_Firmware_Upgrade_Wizard_v4.3.1.1_SRC\FirmwareFiles
  • Refer to the table above to identify the correct UPS firmware file for your UPS





Step 5B

  • Navigate to the "Configuration" Menu, select "Firmware Update", then use the "Choose File" button to browse for the UPS firmware file downloaded and identified in Step 4B.
  • Once the correct UPS firmware file has been selected, click the “Update UPS” button to apply the update.

how to update UPS FW

The below window will open after selecting “Update UPS”

UPS FW update in progress

The update may take several minutes.

Step 6B

  • To verify the UPS firmware version, choose “About”, then “UPS”:


how to check UPS FW
IMPORTANT: after the UPS firmware update is completed, the UPS LCD may display “Communication Error”. Follow the below steps to clear the alarm:

  • Turn off and unplug UPS from AC mains supply.
  • Disconnect the battery.
  • Reconnect the battery, reconnect the UPS to AC mains supply, and turn on the UPS. The UPS will now work normally with the updated firmware.
  • You can now turn the UPS output back on. From the NMC web interface choose “Control”, then “UPS”.
  • “Skip outlet on delays” may be selected if required to restore power immediately:

how to turn on UPS output

For any issues encountered during the update process or any additional questions, please contact APC Tech Support.

Note:
UPS units already having the firmware versions listed in the table below, or later versions, will not have an option to update the UPS firmware through the web interface of the Network Management Card (NMC):
UPS ModelFirmware Version
SRC5KUXI14.0
SRCE6KUXI14.1
SRC6KUXICH14.2
SRC10KUXI14.0
SRC10KUXICH14.1

Schneider Electric Việt Nam

Phần đính kèm
Smart-UPS_Firmware_Upgrade_Wizard_v4.3.1.1_SRC.exe [100.58 MB]
SRC FW Upgrade (CH translation)-V5_updated Oct.31.pdf [1.5 MB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: