Hôm nay chúng tôi có thể giúp gì cho bạn?

What is the insulation resistance and dielectric strength test for BMXXBC008K?

Issue
What is the insulation resistance and dielectric strength test for BMXXBC008K?

Product line
M340 backplane extension cable

Environment
BMXXBC008K

Resolution
The insulation resistance is 20 ohms per kilometer and the dielectric strength is 1500VAC.