Hôm nay chúng tôi có thể giúp gì cho bạn?

What is the maximum number of ATV320 Drives using the VW3A3616 Ethernet card can be wired in daisy chain?

Issue:

ATV320 Drives using the VW3A3616 Ethernet card what is the maximum you can wire in daisy chain?

Product Line:

ATV320 with optional card VW3A3616 Ethernet card.

Environment:

All

Cause:

Max number of devices can be daisy chained.

Resolution:

VW3A3616