Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to resolve corruption errors in historic and alarm summary files
This article helps resolve the following error that may appear for historic granules (.HRD) or alarm summary files (.ALS).

Error

Try these steps:

1. Copy the historic granule into C:\Temp. Do not use Cut and Paste.

2. Launch Windows Command Prompt as a user with the administrator privileges.

3. Type the following command: cd C:\Program Files (x86)\Schneider Electric\ClearSCADA

  • if the above command does not work, try: cd C:\Program Files (x86)\Schneider Electric\Geo SCADA

Navigating to the correct folder

4. Now run the following command. The name of the historic granule in this example is WK021954.HRD. You need to run this command for each historic granule if you have multiple corruption errors:

  • SCXCMD HISINFO "C:\Temp\WK021954.HRD"

5. You should get something in return. See if there are any duplicate entries:

Running HISINFO command

6. If there any Duplicate or Deleted records, please run the HISSTRIP command:

  • SCXCMD HISSTRIP "C:\Temp\WK021954.HRD"

7. The deleted and duplicate records should now show zeros.

8. Shutdown Geo SCADA and copy the cleaned up historic granule back into the correct place in the historian. Start your Geo SCADA backup.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: