Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why "OFSLog" shows the message “Not enough space”?
Some customers observe that the memory space consumed by OFS grows regularly.
At the end, "OFS" doesn't work anymore.  
Customer have to restart the PC to make "OFS" operational again.

print screen

Explanation:
there's a memory fragmentation which has the same effects as a memory leak.
This effect is due to the garbage collector which is active by default and must be deactivated.
On OFS V3.63 SP2, it will be disabled by default and not enabled.

To deactivate the garbage collector, you must therefore:
• stop OFS
• edit C:\ProgramData\Schneider Electric\OFS\3.63.0.0\ofsinternal.xml
• replace <add value="true" key="GarbageCollector"/> by <add value="false" key="GarbageCollector"/>

In the OFS log, we must have Garbage collector is not active

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: